Hi
I have a custom board with KL02 and a P&E Multilink ACP debugger. SWD connections are correct, reset as well.
I always use this board.
After sometime without use when I started debugging the project the P&E Multilink ACP began updating itself. Since then, whenever I try to debug it shows "Connection closed by the GDB server." and popup Runtime error 216 at ...
I checked early recent related posts and it seems this issue is happening in different platforms with P&E or OpenSDA not long ago.
I tried to remove and install the MCUxpresso and the latest P&E driver back again.
With the Freedom board with OpenSDA everything works fine.
By the way, I can erase or program the Flash. Only debugging is the problem.
Closest post I have found is Gdb server closes connection.@Gdb server closes connection.
Please help.
Thank you
Andre VB
Hi
My FRDM-KE02Z40M had the same Runtime error with frdmke02z40m_led_blinky_1.
I've taken care of the PEmicro Blog, but the Runtime error continues.
FYI: In FRDM-KL25Z, I used the same MCUXpresso IDE with NO Runtimetime error without any solution. I'm able to debag without problems.
My environment is Windows 10 v2004, MCUXpressoIDE_11.1.1, FRDM-KE02Z40M SDK 2.8.0 (2020-07-21), FRDM-KL25Z SDK 2.2.0.
Attached 2 figures are the difference in PEmicro Blog.
Thank you.
Hello Andre Luis Vilas Boas
There seems to be an issue between the latest MCUXpresso release and the P&E drivers. MCUXpresso works well with the SEGGER OpenSDA. I suggest you try this IDE configuration http://www.pemicro.com/blog/index.cfm?post_id=130
Please let me know if this post solved the problem.
Best regards,
Omar