RT1060-EVK Unable to program

cancel
Showing results for 
Search instead for 
Did you mean: 

RT1060-EVK Unable to program

178 Views
chadgraham
Contributor IV

Hello,

I have a RT1060-EVK that I cannot connect to with the CMSIS-DAP.  I have tried new workspaces, new examples, different QSPI configuration files, external tools (blhost), and even the Boot utility... all without success.

Looking on the forums, this appears to be a common problem, but none of the suggestions have corrected the issue.  Does anyone have a method to correct this?  The error log is listed below.

MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 16:50:12 - crt_emu_cm_redlink build 18)
Found chip XML file in C:/Work/Designs/TempWorkspace/evkmimxrt1060_iled_blinky/Debug\MIMXRT1062xxxxA.xml
Reconnected to existing LinkServer process.
============= SCRIPT: RT1060_connect.scp =============
RT1060 Connect Script
DpID = 0BD11477
APID = 0x04770041
Disabling MPU
Configure FlexRAM for 768KB OC RAM, 128KB I-TCM, 128KB D-TCM
Finished
============= END SCRIPT =============================
Probe Firmware: CMSIS-DAP (ARM)
Serial Number: 02290000060a94aa00000000000000000000000097969905
VID:PID: 0D28:0204
USB Path: \\?\hid#vid_0d28&pid_0204&mi_03#a&1e662134&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Using memory from core 0 after searching for a good core
debug interface type = CoreSight DP (DAP DP ID 0BD11477) over SWD TAP 0
processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0
number of h/w breakpoints = 8
number of flash patches = 0
number of h/w watchpoints = 4
Probe(0): Connected&Reset. DpID: 0BD11477. CpuID: 00000C27. Info: <None>
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Content of CoreSight Debug ROM(s):
RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)
ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)
ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)
ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)
ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)
ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)
ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)
ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core
ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT
ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU
ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)
NXP: MIMXRT1062xxxxA
DAP stride is 1024 bytes (256 words)
XML Error - no license-type XML file 'crt_common.xme' on path.
note - part information contained no product license-type data
Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID MIMXRT1060_SFDP_QSPI.cfx
Image 'iMXRT1060_SFDP_QSPI Mar 22 2021 08:15:58'
Opening flash driver MIMXRT1060_SFDP_QSPI.cfx
Sending VECTRESET to run flash driver
Driver V.2 dynamic startup failed - driver Init provided no flash parameters
Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters.
Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPIJ driver rc 20107 (0x4E8B)
chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.
failed to initialize flash driver MIMXRT1060_SFDP_QSPI.cfx

0 Kudos
1 Reply

119 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @chadgraham,

As I saw that you use the MCUBootUtility, I think you already try the serial downloader but could you confirm if the method in the following post.

Best Regards,

Alexis Andalon

0 Kudos