Pin# of J1 and J2 on LPCXpresso51U68 (OM40005) dev board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin# of J1 and J2 on LPCXpresso51U68 (OM40005) dev board

520 Views
larry781111
Contributor I

In the sample code "lpcxpresso51u68_COM_cmsis_spi_interrupt_transfer"

On the board only shows D0,D1,D2...D15, they should be match for Arduino Uno

There is no pin# definition about J1 and J2 on the guideline of the dev board, so how can I figure out which pin is J1 pin 11, pin 13, pin 15 and J2 pin 8 

pastedImage_1.png

0 Kudos
2 Replies

422 Views
soledad
NXP Employee
NXP Employee

Hi,

You can find more information in the user manual for this board. 

https://www.nxp.com/webapp/Download?colCode=UM11121&Parent_nodeId=1524171247616709881866&Parent_page... 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

422 Views
larry781111
Contributor I

Hi Sol,

Thanks for your reply, but the manual did not include the pin definition.

I can't even find the first pin of J1#1 in the manual, now I can just trace the pin 1by1.

0 Kudos