PWM trigger DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM trigger DMA

909件の閲覧回数
phuongly1
Contributor I

Hi,

I am using MIMXRT1052. I generated pwm output signals by either flexPwm or by Quarter Timer. I want to use the rising or falling edge of this pwm signal to trigger DMA that reads data from the existing source then writes the data to gpio output pin. I read the MIMXRT1050 reference manual but I could not find the right registers to do this. Please help.

Thank you.

0 件の賞賛
2 返答(返信)

747件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Phuong,

You can try to use QTMR. There is a demo called evkbimxrt1050_qtmr_inputcapture_outputpwm_dma. You can find it in SDK_2.5.0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\qtmr\inputcapture_outputpwm_dma.

It shows 2 function of QTMR. One is capture, the other is pwm. In the pwm part, it use DMA to fill CMPLD register. You can also use it to move data from existing source to destination register.

EDMA_PrepareTransfer(

                            &transferConfig,

                             (uint16_t *)&g_Cmpld1Value,    //source data address

                             2,                                                // width

                             (uint16_t *)&BOARD_QTMR_BASEADDR->CHANNEL[BOARD_QTMR_PWM_CHANNEL].CMPLD1, //destination data address

                             2,

                             2,

                             2,
                             kEDMA_MemoryToPeripheral);

Regards,

Jing

0 件の賞賛

748件の閲覧回数
phuongly1
Contributor I

Thank you for replying my question. Your suggestion is not what I want to do. I would like to use pwm wave form to trigger DMA on every rising or falling edge. Actually, I found the solution on XBARA. I could pass my flexPWM or quart timer to XBARA as input then output to DMA base on rising or falling edge of my signal. Everything is working as I expected now.

Thank you

0 件の賞賛