PN7462AU-FW_v04.01.00.zip link request

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7462AU-FW_v04.01.00.zip link request

1,047 次查看
sachin_singh
Contributor II

Hi All,

I am working on the PN7462AU kit for the contact card - SAM Card and contact less card - Mifare Classic card to perform read and write operation.

For that I had use the Firmware example PN7462AU-FW_v05.07_Full.

I need to read the contact card SAM card as described in the UM10957 Door Access UM.

The firmware file I have it contain only contact less card  door access example, not for the contact card.

But the firmware I am using it was v5 and and in user manual firmware version is v4.

So, Can any one can share me the link for the PN7462AU-FW_v4 to access the  phExDoorAccessEC example.

Looking forward for the response ... !!!

Regards

标签 (1)
0 项奖励
回复
1 回复

958 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

The example is available in the Extended version of the reader library in DocStore, for this it will be necessary to register and have an active NDA with NXP.

BR,

Ivan.

0 项奖励
回复