PN5180 LPCD mode instructions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 LPCD mode instructions

1,769 Views
moises_reyes
Contributor II

Hi there,

I am currently trying to send the chip PN5180 to LPCD mode (auto calibration) from an active mode (card reader poll mode).

As MCU i am using a MK81 processor which send the instructions via SPI bus to the NFC chip. The IDE is MCUExpresso IDE v10.2.0_759 with the NXP library NxpNfcRdLib_5.7.0.

Until now I was no able to find any complete sample code to fulfill this task.

Now I will show you what I have done and the source code related to this matter.

1- The registers mentioned in the data sheet related to LPCD mode are already set. The values readed from chip, (to proof it), are shown now.

   

      ADDR = 34 -> 0x01

      ADDR = 36 -> 0xff

      ADDR = 37 -> 0x05

      ADDR = 38 -> 0x00

      ADDR = 39 -> 0xf0

      ADDR = 3A -> 0xf0

2- The source code, used to send the chip PN5180 to LPCD mode (auto calibration) from an active mode (card reader poll mode), is given now.

///////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

phStatus_t Cl_SwitchMode_to_LPCD()

{

        phhalHw_Pn5180_DataParams_t *cl_pDataParams;

        phacDiscLoop_Sw_DataParams_t *cl_SW_pDataParams;

        phStatus_t status = PH_ERR_SUCCESS;                                    //BP_1

        uint16_t cl_wakeupCounterInMs = 1000;                         

 

        /* Set the generic pointers */

        cl_pDataParams = phNfcLib_GetDataParams(PH_COMP_HAL);

        cl_SW_pDataParams = phNfcLib_GetDataParams(PH_COMP_AC_DISCLOOP);

 

 

        /* Read and print registers values from EEPROM */

        CL_get_LPCD_EE_Values(cl_pDataParams);                                 //BP_2

 

 

        /* Enable LPCD Mode*/

        status = phacDiscLoop_SetConfig(cl_SW_pDataParams, PHAC_DISCLOOP_CONFIG_ENABLE_LPCD, PH_ON);

        if(PH_ERR_SUCCESS== status)

        {

                PRINTF("LPCD_Mode Enable \t-> \tOK\n");                        //BP_3

        }

 

        /* Switch to LPCD Mode*/

        status = phhalHw_Pn5180_Instr_SwitchModeLpcd(cl_pDataParams, cl_wakeupCounterInMs);

        if(PH_ERR_SUCCESS== status)

        {

                PRINTF("Switch_Mode instruction \t-> \tOK\n");                 //BP_4

        }

 

        return status;

}

//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

  • Do you see something out of the place or something missing?
  • Do you have a procedure instructions step by step to achieve this task?
  • Until now, I have found sample codes where the instruction "phhalHw_Pn5180_Instr_SwitchModeLpcd()" is not used, so that is why I am confuse, becouse in the data sheet they mention it as a crusial part of the process.

Please, I am in a hurry so your help is very appreciate.

Many thanks in advance and have a nice day.

Tags (1)
0 Kudos
1 Reply

1,415 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please see below for internal apps team response:

First I would suggest checking the LPCD functionality by NFCCockpit, this way you will get and could set all relevant parameters, guidelines you can find in AN11744 (chapter 4.9) and in Datasheet.

 

After that when you have a working LPCD functionality, you can use test results in the application, don't get me wrong - the same parameters can be defined through embedded application also.

 

Next step would be to open one of the provided application in the PSP (e.g., NfcrdlibEx1_BasicDiscoveryLoop) supporting LPCD.

This example implements LPCD feature in a combination of discovery loop.
Please check next segments in the code:

/* Configure LPCD */         
if ((status & PH_ERR_MASK) == PHAC_DISCLOOP_LPCD_NO_TECH_DETECTED)
{             
   status = phApp_ConfigureLPCD();             
   CHECK_STATUS(status);         
}

/* Bool to enable LPCD feature. */         
status = phacDiscLoop_SetConfig(pDataParams, PHAC_DISCLOOP_CONFIG_ENABLE_LPCD, PH_ON);         
CHECK_STATUS(status);

 

When LPCD is appropriately configured and enabled, the library will automatically handle LPCD.

 

as a result of the discoveryLoop run, you can get "PHAC_DISCLOOP_LPCD_NO_TECH_DETECTED", which tells you that PCD returned success (LPCD triggered), but no technologies were detected during technology detection stage.

 

check this code snipped

else if ((status & PH_ERR_MASK) == PHAC_DISCLOOP_LPCD_NO_TECH_DETECTED)
{
    /* LPCD is succeed but no tag is detected. */
}

  

I hope this will help you to use LPCD in your application.

Best regards,

Ivan.

0 Kudos