The current version of SDK for FRDM-K66F is 2.5. However, in mbed (https://github.com/ARMmbed/mbed-os/tree/master/targets/TARGET_Freescale/TARGET_MCUXpresso_MCUS/TARGE...), the SDK version for FRDM-K66F is 2.2. The SAI code which works in SDK 2.5 does not work in SDK 2.2 in mbed and we have identified that updating SAI/SAI_EDMA drivers in mbed fixes the issues.
Using the SDK building, I am only able to access SDK 2.5. We were planning to release some code with mbed so that it is easier for others to use. But, since the SAI code didn't from the newer version didn't work directly, I wanted to look at example code from SDK 2.2 and change the code accordingly. Could you tell me how to get an older SAI example from SDK 2.2 for K66F?
Solved! Go to Solution.
Hello Sachin BS,
I download and upload it to google drive, please try to get it :
https://drive.google.com/open?id=1VrSEJOH5ofGp29bU3s8U18Mnx1quS37P
Hope it helps,
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Sachin BS,
When download SDK package, we can also choose the old version:
so you can download the SDK2.2 for FRDM-k66 from the below link:
https://mcuxpresso.nxp.com/en/dashboard?uvid=172015
You can also refer to your requirement config options and download.
Hope it helps,
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Alice,
Using the link (https://mcuxpresso.nxp.com/en/dashboard?uvid=172015), I get the following error.
I didn't see any link for SDK version in SDK builder
Hello Sachin BS,
I download and upload it to google drive, please try to get it :
https://drive.google.com/open?id=1VrSEJOH5ofGp29bU3s8U18Mnx1quS37P
Hope it helps,
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------