Hopefully an easy one.
I'm dealing with an apparent messaging issue and I want to see what's in a specific queue, but when I suspend execution (MCUXpresso v11.1.1) I don't get any informatino in the "Queue List (FreeRTOS)" tab except "TmrQ".
I should point out that I've added Erich's code for listing tasks (Tutorial: Using Runtime Statistics with Amazon FreeRTOS V10) but queue information has never been presented.
I did do a search and it seems like when you suspend/pause execution, the queue information should be presented but I've never set it.
Thanx,
myke
Solved! Go to Solution.
Found it - you have to call the FreeRTOS "vQueuAddToRegistry" API after your "xQueueCreate" API call.
If anybody cares, I define a structure with my queue information (along with pointers to the variables storing the handles):
typedef struct makeQueuesStruct {
uint8_t queueName[20];
QueueHandle_t* queueHandlePointer;
UBaseType_t queueElements;
UBaseType_t queueElementSize;
} makeQueues;
makeQueues makeQueuesArray[] =
// "01234567890123456789"
{ { "flashQUEUE\0", &flashQUEUE_Handle, MAKEQUEUES_ELEMENTS, sizeof(struct flashQueueMsg) }
, { "flashRXQUEUE\0", &flashRXQUEUE_Handle, MAKEQUEUES_ELEMENTS, sizeof(struct flashQueueMsg) }
, { "panelQUEUE\0", &panelQUEUE_Handle, MAKEQUEUES_ELEMENTS, sizeof(struct panelQueueMsg) }
//... and so on through all the Queues
, { "\0", NULL, 0, 0 }
};
and then read through it, create the queues and then add to the registry:
for (i = 0; '\0' != makeQueuesArray[i].queueName[0]; ++i) {
if (0 == (*makeQueuesArray[i].queueHandlePointer
= xQueueCreate(makeQueuesArray[i].queueElements
, makeQueuesArray[i].queueElementSize))) {
#if (2 != SDK_DEBUGCONSOLE)
PRINTF("Unable to Create \"%s\"\n"
, makeQueuesArray[i].queueName);
#endif
for (;;) { }
}
else {
vQueueAddToRegistry(*makeQueuesArray[i].queueHandlePointer
, (const char*)makeQueuesArray[i].queueName);
}
}
Works nicely and immediately helped me identify my error (two tasks that are blocked waiting for replies from each other - I didn't think through on one execution workflow).
Found it - you have to call the FreeRTOS "vQueuAddToRegistry" API after your "xQueueCreate" API call.
If anybody cares, I define a structure with my queue information (along with pointers to the variables storing the handles):
typedef struct makeQueuesStruct {
uint8_t queueName[20];
QueueHandle_t* queueHandlePointer;
UBaseType_t queueElements;
UBaseType_t queueElementSize;
} makeQueues;
makeQueues makeQueuesArray[] =
// "01234567890123456789"
{ { "flashQUEUE\0", &flashQUEUE_Handle, MAKEQUEUES_ELEMENTS, sizeof(struct flashQueueMsg) }
, { "flashRXQUEUE\0", &flashRXQUEUE_Handle, MAKEQUEUES_ELEMENTS, sizeof(struct flashQueueMsg) }
, { "panelQUEUE\0", &panelQUEUE_Handle, MAKEQUEUES_ELEMENTS, sizeof(struct panelQueueMsg) }
//... and so on through all the Queues
, { "\0", NULL, 0, 0 }
};
and then read through it, create the queues and then add to the registry:
for (i = 0; '\0' != makeQueuesArray[i].queueName[0]; ++i) {
if (0 == (*makeQueuesArray[i].queueHandlePointer
= xQueueCreate(makeQueuesArray[i].queueElements
, makeQueuesArray[i].queueElementSize))) {
#if (2 != SDK_DEBUGCONSOLE)
PRINTF("Unable to Create \"%s\"\n"
, makeQueuesArray[i].queueName);
#endif
for (;;) { }
}
else {
vQueueAddToRegistry(*makeQueuesArray[i].queueHandlePointer
, (const char*)makeQueuesArray[i].queueName);
}
}
Works nicely and immediately helped me identify my error (two tasks that are blocked waiting for replies from each other - I didn't think through on one execution workflow).