No probes found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No probes found

2,557 Views
timg
Contributor I

No available probes

Running MacOS mojave 10.14. MCUXpresso 10.3 Freedom K66 board using USB

This used to work in previous MCUXpresso and MacOS. I hadn't tried to connect in a while.

What other information would help?

Can anyone help me?

Thank you

Tim

0 Kudos
2 Replies

2,193 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Tim:

I would suggest you delete the existing launch configuration , then a debug probe discovery operation will be automatically performed to display the available debug connections.

Please refer to below link for more details.

https://community.nxp.com/docs/DOC-335463 

Regards

Daniel

0 Kudos

2,193 Views
timg
Contributor I

When powered with the USB in the debug port the yellow LED flashes quickly.

Also, tried using J-Link to connect got

SEGGER J-Link Commander V6.40 (Compiled Oct 26 2018 15:07:23)

DLL version V6.40, compiled Oct 26 2018 15:07:12

Connecting to J-Link via USB...FAILED: Cannot connect to J-Link via USB.

0 Kudos