No probes discovered

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No probes discovered

701 Views
stirbu_rares
Contributor I

Hello,

I recently received an OM13094 LPCXpresso54618 CAN-FD kit.

I downloaded (what i believe is ) the last version for MCUXpresso ID, to be more specific v10.3.1.

When i try to debug my code i receive the following error:

pastedImage_2.png

I tried reinstalling everything, updated the software, changed the J-Link Server executable to JLinkGDBServerCL.exe ( note i am using JLink_V642b), and i still don't know what may be the problem.

A little help would be strongly appreciated.

0 Kudos
4 Replies

604 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

You meet connection problem. The problem may be in either project itself or board firmware.

- project itself.

thus, please create a NEW project in a NEW workspace, test connection

 

- on board debug firmware.

I suggest you refer this link to 

https://community.nxp.com/thread/456242 

update the firmware. I suggest you also check CMSIS-DAP interface.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

604 Views
stirbu_rares
Contributor I

Hello,

Thanks for the advice, sadly none of them seem to work.

I used the link you suggested.

I know for sure that in "device and printers" there should be my board labeled "LPC", sadly i do not see it, i believe that is the cause of the problem.

0 Kudos

604 Views
converse
Senior Contributor V

Make sure you are connected to a USB port that is capable of supplying sufficient power to your board. Often, you can change the amount of power supplied to the USB port through the properties of the USB Root Hub in the Device Manager. Failing that, try other USB ports.

Also, make sure your USB cable is working - they fail surprisingly frequently.

0 Kudos

604 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Stirbu Rares,

I have a customer met similar problem as yours.

He finally fixed his problem by changing another computer.

So I suggest you test your board connection issue another another computer to verify if the problem is on your computer system. Can you please test?


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos