No compatible probes available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No compatible probes available

2,083件の閲覧回数
kunalpatil
Contributor I

Hello NXP, I downloaded the new MCUXpresso IDE v10.1.0. I can build a project but when I click on Flash 'LPCXpresso1769 CMSIS-DAP board’, I get an error message – “No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target”.  I have checked the board where the jumper is supposed to go and also I have installed necessary drivers.

タグ(1)
0 件の賞賛
返信
1 返信

1,288件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Kunal,

What operating system do you work with?

officially we support:

Host operating systems:
 Microsoft® Windows® 7/8/10
Ubuntu Linux® (64 bit)
Mac OS X 10.11 and later

Please refer User guide "16.9 Using and troubleshooting LPC-Link2 " for trouble shooting:

https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf 

Refer this discussion to update board interface in case on board interface firmware is damaged.

LPC54608 board doesnt see any debug probes  


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信