Hello everyone, I am super new to MCUXpresso. I have recently purchased LPC1769 and cannot get a basic program to run. I am getting "No compatible probes available" error when trying to debug.
I have seen a similar question asked here I tried doing every step but I still couldnt get the program to work.
I am using Windows 10.
The device, when connected starts to blink the on-board LEDs (which gives me hope that nothing is actually wrong with the board itself).
In Control Panel > Devices and Printers it shows up as MBED CMSIS-DAP.
I tried running LPCScrypt, but it gives me Nothing to boot message. I also tried these steps with both shorted and un-shorted JP3.
I have indicated "MCU Linker Script" to be Redlib (semihost) (not entirely sure if this has anything to do with it)
I am really confused. Any help would be appreciated.
Hello ,
Please refer to the thread the below thread to update firmware:
Pay attention, when update debug probe firmware, not to press press reset button, it should "short the two pads at jumper 4 (JP4) to put LPC11U35 in ISP mode", detail please check that thread.
BTW, there is lpcopen support this board, it includes drivers and demos, download from:
BR
Alice