We are working on a new board using MCUXpresso IDE and the KE02Z16VLD4 processor. I built the SDK on the website and added a few things (the UART fsl driver and debug). However, I noticed when I built it in the MCUXepresso it used up over 80% of the flash memory. I looked at the UART source and it has a lot of stuff I don't need (all I need it for is diagnostic output) Can I remove the fslUart driver while in the IDE? Or do I have to go back and regenerate a new SDK (which I hope I don't have to each time I want to change something?)
Thanks,
Bill
Found it - right click on project and the option is Manage SDK Components