Migrating a project from LPCXpresso to MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Migrating a project from LPCXpresso to MCUXpresso

3,713 Views
TomLaVecchia
Contributor II

I inherited a LPCXpresso project which runs on a LPC1769 board. I tried to move it to MCUXpresso and was able to get it to compile after a couple errors. Now when I try to download it to the board it downloads however it doesn't run, any suggestions on what I might be missing?

0 Kudos
Reply
5 Replies

3,709 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello TomLaVecchia,

Which project? You can send your original project to me ,  I help to check it on my side.

 

BR

Alice

0 Kudos
Reply

3,697 Views
TomLaVecchia
Contributor II

At this time, I cannot send it to you. I'm trying to get approval to send it.

My next question is, should I have been able do just import the LPCXpresso project into MCUXpresso or did I need to start a new project under MCUXpresso and then just copy the code into the folder?

Tags (1)
0 Kudos
Reply

3,682 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello TomLaVecchia,

Usually, we can directly import and open it with MCUXpresso IDE.

You can also create a private case in salesforce and send your project.: https://support.nxp.com/s/  

Choose LPC space, and also can add this thread linker in description, I will help you to test it on my side.

 

BR

Alice

 

0 Kudos
Reply

3,670 Views
TomLaVecchia
Contributor II

I can't send the entire project including code,

Is there another way we can work on this? Can I just send a configuration file or something?

 

Tags (1)
0 Kudos
Reply

3,651 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello TomLaVecchia,

Without project, it hard find the issue, I saw you have create new case on salesforce, you can attach some compile error .

 

BR

Alice

0 Kudos
Reply