Migrating a project from LPCXpresso to MCUXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Migrating a project from LPCXpresso to MCUXpresso

3,727件の閲覧回数
TomLaVecchia
Contributor II

I inherited a LPCXpresso project which runs on a LPC1769 board. I tried to move it to MCUXpresso and was able to get it to compile after a couple errors. Now when I try to download it to the board it downloads however it doesn't run, any suggestions on what I might be missing?

0 件の賞賛
返信
5 返答(返信)

3,723件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello TomLaVecchia,

Which project? You can send your original project to me ,  I help to check it on my side.

 

BR

Alice

0 件の賞賛
返信

3,711件の閲覧回数
TomLaVecchia
Contributor II

At this time, I cannot send it to you. I'm trying to get approval to send it.

My next question is, should I have been able do just import the LPCXpresso project into MCUXpresso or did I need to start a new project under MCUXpresso and then just copy the code into the folder?

タグ(1)
0 件の賞賛
返信

3,696件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello TomLaVecchia,

Usually, we can directly import and open it with MCUXpresso IDE.

You can also create a private case in salesforce and send your project.: https://support.nxp.com/s/  

Choose LPC space, and also can add this thread linker in description, I will help you to test it on my side.

 

BR

Alice

 

0 件の賞賛
返信

3,684件の閲覧回数
TomLaVecchia
Contributor II

I can't send the entire project including code,

Is there another way we can work on this? Can I just send a configuration file or something?

 

タグ(1)
0 件の賞賛
返信

3,665件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello TomLaVecchia,

Without project, it hard find the issue, I saw you have create new case on salesforce, you can attach some compile error .

 

BR

Alice

0 件の賞賛
返信