McuxPresso Binary file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

McuxPresso Binary file

ソリューションへジャンプ
4,335件の閲覧回数
claudiobrunelli
Contributor II

Hi

I have just created a new test proget with the xpresso ide. In the attached file ther's the corresponding binary file and a little screenshot of it.

Does anyone to explain me why I find in this file the information that I lighted ? Is this correct to find this kind of information in the binary file ? Is there any setting to make to avoid it ?

Thanks in advance.

Claudio

0 件の賞賛
返信
1 解決策
4,329件の閲覧回数
ErichStyger
Specialist I

Hi @claudiobrunelli ,

>>Does anyone to explain me why I find in this file the information that I lighted ?

Yes. It is because you have asserts enabled in your project.

 

>>Is this correct to find this kind of information in the binary file ?

Yes. Because you are using asserts the way it is implemented in the SDK

 

>>Is there any setting to make to avoid it ?

Yes, disable asserts with the NDEBUG setting. See https://mcuoneclipse.com/2016/03/09/dealing-with-code-size-in-kinetis-sdk-v2-x-projects/

 

PS: There is a nice hex editor plugin in Eclipse too. Have a look at https://mcuoneclipse.com/2012/04/02/5-best-eclipse-plugins-4-ehep/

 

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,330件の閲覧回数
ErichStyger
Specialist I

Hi @claudiobrunelli ,

>>Does anyone to explain me why I find in this file the information that I lighted ?

Yes. It is because you have asserts enabled in your project.

 

>>Is this correct to find this kind of information in the binary file ?

Yes. Because you are using asserts the way it is implemented in the SDK

 

>>Is there any setting to make to avoid it ?

Yes, disable asserts with the NDEBUG setting. See https://mcuoneclipse.com/2016/03/09/dealing-with-code-size-in-kinetis-sdk-v2-x-projects/

 

PS: There is a nice hex editor plugin in Eclipse too. Have a look at https://mcuoneclipse.com/2012/04/02/5-best-eclipse-plugins-4-ehep/

 

I hope this helps,

Erich

0 件の賞賛
返信
4,321件の閲覧回数
claudiobrunelli
Contributor II

Hi ErichS

As usual, your tips & tricks are very very precious.

Thanks

Claudio

0 件の賞賛
返信
4,300件の閲覧回数
ErichStyger
Specialist I

Hi @claudiobrunelli ,

thanks you :-).

To add to the answer: there reasons for the strings are the asserts which use things like __FILE__ and __LINE__ for the printf() messages: they get stored in FLASH.

Erich

0 件の賞賛
返信