MCUxpresso warning - how to resolve

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUxpresso warning - how to resolve

4,522 Views
jefffieldhouse
Contributor I

MCUxpresso is giving this warning: 

"Unable to find device package for project ..."

I'm not sure what exactly it means or how to fix it. I've been working on this project for quite some time and this message came up only within the last little while. I am still able to load and run the project on the target.

Does anyone have any advice or guidance on how to resolve this?

Jeff

8 Replies

3,753 Views
bowerymarc
Contributor V

If you click right on Project Settings -> MCU you can add a package type

0 Kudos
Reply

4,117 Views
lucasrangit
Contributor III

I figured out the issue.

My .cproject file did not have the "package" field. It was also missing "boardID", "core", and "coreID", so I added those to match was I was using (e.g. "MK22FN512VMP12").

        <storageModule moduleId="com.nxp.mcuxpresso.core.datamodels">
                <sdkName>SDK_2.x_FRDM-K22F-OM13588</sdkName>
                <sdkExample>frdmk22f_dev_composite_hid_mouse_hid_keyboard_lite_bm</sdkExample>
                <sdkVersion>2.6.0</sdkVersion>
                <sdkComponents>middleware.usb.device_controller_khci.MK22F51212;middleware.usb.device.MK22F51212;platform.drivers.smc.MK22F51212;device.MK22F51212_CMSIS.MK22F51212;platform.Include_common.MK22F51212;platform.Include_core_cm4.MK22F51212;platform.drivers.clock.MK22F51212;platform.drivers.common.MK22F51212;device.MK22F51212_startup.MK22F51212;platform.drivers.lpuart.MK22F51212;platform.drivers.uart.MK22F51212;platform.drivers.gpio.MK22F51212;platform.utilities.assert.MK22F51212;component.lists.MK22F51212;component.serial_manager.MK22F51212;utility.debug_console.MK22F51212;component.uart_adapter.MK22F51212;component.serial_manager_uart.MK22F51212;platform.drivers.port.MK22F51212;middleware.baremetal.MK22F51212;frdmk22f_dev_composite_hid_mouse_hid_keyboard_lite_bm;</sdkComponents>
                <boardId>frdmk22f</boardId>
                <package>MK22FN512VLH12</package>
                <core>cm4</core>
                <coreId>core0_MK22FN512xxx12</coreId>
        </storageModule>

It is a bug that these are not added to the .cproject file by the new IDE when upgrading the project files. They are present in the SDK example projects.

0 Kudos
Reply

4,117 Views
lucasrangit
Contributor III

Having the same problem after upgrading SDK to 2.6.0. I did not encounter this issue after upgrading to MCUXpresso 11.0 with my 2.4.1 SDK (using a FRDM-K22F).

eclipse.buildId=unknown
java.version=1.8.0_201
java.vendor=Oracle Corporation
BootLoader constants: OS=linux, ARCH=x86_64, WS=gtk, NL=en_US
Command-line arguments: -os linux -ws gtk -arch x86_64 -data /home/vagrant/workspace

com.nxp.mcuxpresso.core.datamodels
Warning
Thu Jun 20 15:03:59 GMT+02:00 2019
Unable to find device package for project 'frdmk22f_om13588_project'.

0 Kudos
Reply

4,117 Views
BlackNight
NXP Employee
NXP Employee

I do have as well 2.4.x SDK versions, but on my end the following helped:

pastedImage_1.png

Can you try this (if not already)?

I hope this helps,

Erich

0 Kudos
Reply

4,117 Views
henninjw
Contributor II

I am running into this problem. Was a solution every found?

Thanks!

0 Kudos
Reply

4,118 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jeff,

At what point do you see this warning? Could you post a screenshot of it?

Does this only happen with that specific project?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

4,118 Views
eflament
Contributor II

Carlos,

I get the same error.  If I click on any tab other than "errors", I get brought back to the errors tab with about five new entries about not having the device package for the project.  I have the SDK installed as you can see in my project explorer.  I've selected the MCU under the MCU page of the project settings and also under the devices tab of the c/c++ settings.  I believe the latter is the one the actually starts it off throwing the error.  Also, MCUXpresso config tools, despite all these setups, still starts off with the wrong board selected.

Capture.PNG

-Eric

0 Kudos
Reply

2,145 Views
danielholala
Senior Contributor II

Just came across this 5 year old posting that shows a "Workspace Log":

 

danielholala_0-1687424713973.png

 

I wondered how you open this "Workspace Log". 

The answer is: you have to open the aptly named "Error Log" in Window > Show View > Other dialog.

danielholala_1-1687424871773.png

Hope that helps anybody who has the same question.

0 Kudos
Reply