This is my first time using MCUXpresso Config Tools. I downloaded the SDK file according to the video in the Quick Start, but the following error occurred. I don’t know why, I hope someone can help me
已解决! 转到解答。
Hello,
what IDE are you using? The first options is meant for (already) created project in the IAR, Keil, etc. You should not point it to the downloaded SDK. The standalone Config Tools does not allow open configuration from MCUXpresso IDE.
If you use the MCUXpresso IDE, it can create a project for you and it also contains the Config Tools integrated.
From the screenshot it seems that you are using the tools version 4.0. Since May there is newer version 4.1 which I recommend to use.
Regards,
Libor
Hi Jason.
In addition of Libor, if you want to create a new configuration with standalone Config Tool,
For detail, see attached video.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
what IDE are you using? The first options is meant for (already) created project in the IAR, Keil, etc. You should not point it to the downloaded SDK. The standalone Config Tools does not allow open configuration from MCUXpresso IDE.
If you use the MCUXpresso IDE, it can create a project for you and it also contains the Config Tools integrated.
From the screenshot it seems that you are using the tools version 4.0. Since May there is newer version 4.1 which I recommend to use.
Regards,
Libor