I'm compiling my /src_app folder to Flash2 section in the flash.
What I did is
Added following flash sections:
* MFlash32 | Flash | 0x0 | size=0x1ffc
* Flash_00 | Flash2 | 0x1ffc | size=0x4
* Flash_01 | Flash3 | 0x2000 | size=0x5ffc
* Flash_02 | Flash4 | 0x7ffc | size=0x4
* RamLoc8 | RAM | 0x10000000 | size=0x2000
Added "Extra Managed Linker Script input sections:
* Input section description | Region | Section Type
* */src_app/*.o (.text .text*) | Flash2 | .text
But the linker file comes up with two errors.
Description Resource Path Location Type
no viable alternative at input '/' LPC11A14_bootloader_Debug.ld /LPC11A14_bootloader/Debug line: 38 /LPC11A14_bootloader/Debug/LPC11A14_bootloader_Debug.ld GNU Linker Script Problem
no viable alternative at input '*' LPC11A14_bootloader_Debug.ld /LPC11A14_bootloader/Debug line: 38 /LPC11A14_bootloader/Debug/LPC11A14_bootloader_Debug.ld GNU Linker Script Problem
GCC can handle it, but MCUXpresso makes the errors.
So what should I do?
Best regards
Jesper
Solved! Go to Solution.
See section 18.7 from User Guide. There's an MCUXPresso IDE linker script parser used for nicer formatting. In your case, the parser fails to correctly parse the ld file but, given that the linker doesn't find anything wrong, this means it's a problem with our parser.
Please attach the full linker script file and we'll look into this.
You also have the option to disable linker script editor awareness - see User Guide.
Regards,
MCUXpresso IDE Support
Thanks for a quick responce here is my linker script file.
The error occurs at line 22, in this version.
Description Resource Path Location Type
no viable alternative at input '/' Bootloader_test_Debug.ld /Bootloader_test/Debug line: 22 /Bootloader_test/Debug/Bootloader_test_Debug.ld GNU Linker Script Problem
no viable alternative at input '*' Bootloader_test_Debug.ld /Bootloader_test/Debug line: 22 /Bootloader_test/Debug/Bootloader_test_Debug.ld GNU Linker Script Problem
Maybe the error don't occur until you open the file, but then it will remove the extra flash sections.
Best regards
Jesper M Madsen
See section 18.7 from User Guide. There's an MCUXPresso IDE linker script parser used for nicer formatting. In your case, the parser fails to correctly parse the ld file but, given that the linker doesn't find anything wrong, this means it's a problem with our parser.
Please attach the full linker script file and we'll look into this.
You also have the option to disable linker script editor awareness - see User Guide.
Regards,
MCUXpresso IDE Support