MCUXpresso IDE don't run with Error message after install PN7462AU Software plugin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE don't run with Error message after install PN7462AU Software plugin

1,331 Views
won2rang
Contributor II

MCUXpresso IDE don't run with Error message after install PN7462AU Software plugin.

Tools return "Invalid Configuration" with "Unique configuration settings not found (). Exiting"

How can i fix this error?

MCUXpress : MCUXpresso IDE v11.0.1_2563

plugin is com.nxp.pn7xxxxx.update-8.0.0-SNAPSHOT-163

0 Kudos
Reply
2 Replies

1,229 Views
lpcxpresso_supp
NXP Employee
NXP Employee

You cannot import old LPCXpresso patches into MCUXpresso IDE - which its sounds like you are trying to do. However I believe that the functionality this patch includes is probably already included inside MCUXpresso IDE.

However I would strongly recommend that you look at the documentation provided for PN74xx to check what version of the IDE they actually recommend for use with their software.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

1,229 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

My name is Sabina and I'll be happy to help you. Could you please provide screenshot of the error you are seeing. Also could you confirm if you have imported the project dependecies as well?

Best Regards,

Sabina

0 Kudos
Reply