MCUXpresso IDE下载算法

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE下载算法

823 Views
fovvdk
Contributor II

MCUXpresso IDE如何添加下载算法

0 Kudos
Reply
1 Reply

617 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi chao hu 

MCUXpresso will automatically set up the debug configuration with the needed algorithm for the MCU selected. You can manually change depending in the Debugging interface that you are using with the "debug configuration" option. I recommend you checking the 11.1.1 Debug Launch of the User Guide document located in the path  C:\nxp\MCUXpressoIDE_Version


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply