SDK_2.x_MKL16Z256xxx4
MCUXpresso IDE v10.2.1 [Build 795] [2018-07-25]
In the IDE I used the Config Tool to generate my peripherals.c and peripherals.h files.
When the project is compiled, the structures UART_1_config, UART_2_config, and LPSCI_1_config have compile errors:
../board/peripherals.c:66:4: error: 'uart_config_t {aka const struct _uart_config}' has no member named 'idleType'
../board/peripherals.c:144:4: error: 'lpsci_config_t {aka const struct _lpsci_config}' has no member named 'idleLineType'
I am guessing that the Config Tool is generating code for a version of the SDK that does not match my installed SDK.
How do I sort this out?
Thanks,
Bruce
Solved! Go to Solution.
I got the latest MKL16Z4 MCUXpresso SDK from the web site. It is shows the
version as 2.2.0. See below
Are you suggesting that I download the SDK for the wrong MCU?
What good will that do me?
Thanks,
Bruce
Hardware Details
Included Part Numbers
MKL16Z256VLH4, MKL16Z256VMP4
Board(s)
FRDM-KL46Z
Device
MKL16Z4
Core Type / Max Freq
Cortex-M0P / 48MHz
Device Memory Size
256 KB Flash
32 KB RAM
SDK Details
SDK Version:
2.2.0 (released 2017-03-21)
Host OS:
Windows
Toolchain:
MCUXpresso IDE
Middleware:
CMSIS DSP Library FatFS USB stack FreeRTOS
My ADC does not appear to work on my MKL16Z with the project setup as a MKL26Z.
I attempted to switch the project back to a MKL16Z by editing the MCU, but that left old MKL26Z files in the project, and did not add MKL16Z files.
How do I switch back to the MKL16Z and an SDK that works with the MKL16Z?
Thanks,
Bruce
Sorry for my late reply!
It was caused by the version of SDK_2.x_MKL16Z256xxx4 is too old.
The newer SDK of KL26 will not get this error.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I switched the project from the MKL16Z to the MKL26Z (MKL16Z is the actual
MCU), and replacing the SDK 2.2.0 with SDK 2.4.1.
This required a lot of changes to the project, but it builds without errors
or warnings.
Thanks for the suggestion.
Bruce
On Tue, Jan 15, 2019 at 8:57 AM Bruce Graham <bgraham@technosofteng.com>
I got the latest MKL16Z4 MCUXpresso SDK from the web site. It is shows the
version as 2.2.0. See below
Are you suggesting that I download the SDK for the wrong MCU?
What good will that do me?
Thanks,
Bruce
Hardware Details
Included Part Numbers
MKL16Z256VLH4, MKL16Z256VMP4
Board(s)
FRDM-KL46Z
Device
MKL16Z4
Core Type / Max Freq
Cortex-M0P / 48MHz
Device Memory Size
256 KB Flash
32 KB RAM
SDK Details
SDK Version:
2.2.0 (released 2017-03-21)
Host OS:
Windows
Toolchain:
MCUXpresso IDE
Middleware:
CMSIS DSP Library FatFS USB stack FreeRTOS