MCUExpress IDE 11.0 Unusable on Debian based Linux Distros?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUExpress IDE 11.0 Unusable on Debian based Linux Distros?

1,330 Views
keith_mcrae
Contributor I

MCUExpresso IDE relies on Flexera DownloadManager which is provided as a RPM package. The help instructions say that this is only available on MacOS, Windows and Red Hat based Linux distributions. MCUExpresso IDE instructions say it will work on "any" Linux platform. 

Thanks and regards

Keith McRae

0 Kudos
Reply
2 Replies

1,190 Views
lpcxpresso_supp
NXP Employee
NXP Employee

You don't need to use the Flexera Download Manager - in fact I would recommend you don't try. Just click on the installer that you want to download directly within the web page:

pastedImage_1.png

Sorry if this isn't that obvious, though we are looking into improving the download system used to supply MCUXpresso IDE installers in the future.

Regards,

MCUXpresso IDE Support.

0 Kudos
Reply

1,190 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Elaine,

The linux supported versions for MCUXpresso is Ubuntu 16.04 LTS and later LTS, Only 64-bit versions of Linux but there's the following note in the installation guide.

pastedImage_1.png

It could work in other Linux distributions but was only been tested in Ubuntu.

I hope this helps you.

Best Regards,

Alexis Andalon

0 Kudos
Reply