MCU expresso KL16Z128 cop driver support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU expresso KL16Z128 cop driver support

802 Views
amaciuszonek
Contributor I

Hello, is there a timeline to have support for the cop in this micro via the peripheral configuration tool?

0 Kudos
Reply
2 Replies

729 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Artur,

 

Thank you for reporting this issue. As a temporary workaround you can copy the cop drivers from a different SDK (MKL16Z64 for example) and paste them in the following path.

 

SDK_2.2.0_MKL16Z128xxx4.zip\devices\MKL16Z4\drivers

 

This way you will be able to include the drivers through the SDK management window.

 

I hope this helps.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

729 Views
amaciuszonek
Contributor I

Hello Felipe, I will try that and let you know in a few days.

0 Kudos
Reply