How do I set the line spacing in the built-in text editors?
I have a certain program that whenever I scroll past line 550, it quadruples the line spacing, and it remains that way.
I would just like to return it to the standard value.
解決済! 解決策の投稿を見る。
Unfortunately, that doesn't work if the errant character was introduced using an earlier version of MCUXpresso without the bug!
Could the be a control character in the file around line 550? I have much larger files and have no such problem.
It could be due to this Eclipse bug report caused by multi-byte characters.
https://bugs.eclipse.org/bugs/show_bug.cgi?id=206740
Thanks,
That’s the one. I had a Σ in the comment field where I was doing linear regression.
it upset a PC running the latest version of MCUXpresso, but my laptop which was running an older version on Linux was quite happy.
There also seems to be a bug in this forum software. It lets me type the reply, then asks me to log in, then tells me that an unexpected error occurred and loses what I typed, so that I have to type it again.
Re the forum bug: the workaround is to use the Back button in the browser - pressing twice should take you back to your typing, so you don’t lose anything! Annoying, but it saves a lot of retuning!
Unfortunately, that doesn't work if the errant character was introduced using an earlier version of MCUXpresso without the bug!
never seen something like this. Can you share some more details (version of IDE, host, ...)?
Does it happen for every file or just for one?