MCU Xpresso 11.1.1 --- restart debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU Xpresso 11.1.1 --- restart debugging

1,083 Views
zhang2018tz
Contributor I

I am working on a RT600 dev board (evkmimxrt685) and a LPC55S69 dev board (lpcxpresso55s69) recently, both programming and debugging in MCU Xpresso 11.1.1.

When debugging LPC55S69, after I download the code, I can resume, pause, and also click the "restart" button to go back running from "main".

But I can NOT do "restart" with the RT600. RT600 has the same CM33 core as LPC55S69. Each time, after debugging has been started, if I click "restart", and resume, PC goes to a bad position.

So, in short, can anybody load the "dsp_hello_world_usart_cm33" demo of RT600, and successfully do "restart and then resume" in debugging?

Or is there any place (in project setting ...) that I should look into to check for things like "reset setting" "init script" ?

0 Kudos
Reply
1 Reply

987 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Zhang,

yes, this is really a problem. We are investigating now. Sorry for the inconvenience.

Regards,

Jing

0 Kudos
Reply