MCU Linker error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,781件の閲覧回数
jonathansmith
Contributor III

When running MCU Linker in MCUxpresso I get the following error:
arm-none-eabi-gcc.exe: error: false: No such file or directory
/bin/sh: Default: command not found
make: *** [GFM_m0.axf] Error 127

This seems to be becuase the arm-none-eabi-gcc command has the following options specified: arm-none-eabi-gcc -nostdlib -L"C:\GL4K_refresh\LPC4333\lpc_chip_43xx_m0\Debug" -Xlinker -Map="GFM_m0.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -mcpu=cortex-m0 -mthumb -T "GFM_m0_Debug.ld" false; Default -o "GFM_m0.axf"  

A similar project doesn't have the false; Default flag specified and it compiles okay.

Can anyone help me with how to remove these options from the link script? I can't work out where they are set.

Many thanks

0 件の賞賛
返信
1 解決策
2,609件の閲覧回数
jonathansmith
Contributor III

Solved it by updating to the latest version of MCUxpresso.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,610件の閲覧回数
jonathansmith
Contributor III

Solved it by updating to the latest version of MCUxpresso.

0 件の賞賛
返信