MC9S12XDP512 Secure Mode Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S12XDP512 Secure Mode Issue

419 次查看
okan_saglam
Contributor I

Hello,

I am trying to use MC9S12XDP512 microcontroller in secure mode. The application code runs without any issues in unsecure mode, but when secure mode is enabled, I encounter a problem.

Based on my observations, the issue occurs when accessing variables in the SRAM region. These variables are located in the 0x20_0000–0x3F_FFFF (CS1) area. When secure mode is active, the program unexpectedly stops running.

Is there any special configuration required for SRAM access in secure mode?
Do you have any suggestions?

Best regards.

0 项奖励
回复
1 回复

395 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

It does not smell me like security issue but something between debug and normal mode together with writing mode register twice (it is write once only in the normal mode).

BTW, do not you mix security and protection?

https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-S12XE-External-BUS-design-Addendum-To...

 

Please read AN-ExBUS-AddendumToAN2708-v.0.2.zip chapter 5.2 SW Solution from the page and compare design.

I believe you will find the source of the issue because I do not see into your HW and SW design.

 

Best regards,

Ladislav

0 项奖励
回复