Linker warning wchar

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,741件の閲覧回数
pluyckx
Contributor I

Hi,

We are using the SDK created by the SDK builder (https://mcuxpresso.nxp.com/en/builder) for the LPC54607 processor. In this SDK, there is a library called fsl_power_lib. This library is built with a wchar of 32 bits.

We are using IAR 7.80.4. It uses a wchar of 16 bits and we want to fix this warning, but not by ignoring it. Is it possible to make the library available with a wchar of 16 bits (so compiled with IAR 7.80.4 for example)? Or give us the source of this library so we can compile it ourself?

At this moment we are not able to upgrade to IAR 8.x because some of our tools are not yet compatible with the new IAR version.

Kind regards,

Philip Luyckx

0 件の賞賛
返信
1 解決策
2,618件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Philip Luyckx,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Please check the attachment.
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

元の投稿で解決策を見る

2 返答(返信)
2,619件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Philip Luyckx,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Please check the attachment.
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
2,618件の閲覧回数
pluyckx
Contributor I

Thank you. The library in the attachments solves the warning.

0 件の賞賛
返信