LPCopen LWIP tcp echo None Response[SOLVED]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCopen LWIP tcp echo None Response[SOLVED]

2,082 次查看
ramazan_kurban3
Contributor III

Hi. I try to operate lwip_tcpecho_sa examples without freertos. when dhcp is inactive, given ip,gw and mask is sended to uart port. TCP is default 7 in code (ı am not sure for that ? ). I ping this ip and this response is coming "target  host unreachable". I cant open tcp server with putty or hercules. 

when dhcp is active, ip is not set and sended default 0.0.0.0. 

Cables and component is true, ı checked it with easyweb examples.

I use mcuexpresso and ı have custom board with lpc1769.

How can ı solve this problem , Which settings should be made ?

标记 (3)
0 项奖励
回复
2 回复数

1,884 次查看
pablog33
Contributor I

Could You solve this? I am having the same problem

0 项奖励
回复

1,906 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Ramazan,

 

Do you need still help with this question? I see you changed the title as solved. Maybe you can share your results with the community.

 

Best regards,

Felipe

0 项奖励
回复