/*
* Copyright 2017 NXP
* All rights reserved.
*
*
* SPDX-License-Identifier: BSD-3-Clause
*/
#include "fsl_debug_console.h"
#include "fsl_device_registers.h"
#include "fsl_spi.h"
#include "fsl_spi_dma.h"
#include "fsl_dma.h"
#include "pin_mux.h"
#include "board.h"
#include <stdbool.h>
#include "fsl_power.h"
/*******************************************************************************
* Definitions
******************************************************************************/
#define EXAMPLE_SPI_SLAVE SPI8
#define EXAMPLE_SPI_SLAVE_IRQ LSPI_HS_IRQn
#define EXAMPLE_SPI_SSEL 1
#define EXAMPLE_DMA DMA0
#define EXAMPLE_SPI_SLAVE_RX_CHANNEL 2
#define EXAMPLE_SPI_SLAVE_TX_CHANNEL 3
#define EXAMPLE_SLAVE_SPI_SPOL kSPI_SpolActiveAllLow
#define TRANSFER_SIZE 4U /*! Transfer dataSize */
/*******************************************************************************
* Prototypes
******************************************************************************/
static void SPI_SlaveUserCallback(SPI_Type *base, spi_dma_handle_t *handle, status_t status, void *userData);
static void EXAMPLE_SlaveInit(void);
static void EXAMPLE_SlaveDMASetup(void);
static void EXAMPLE_SlaveStartDMATransfer(void);
static void EXAMPLE_TransferDataCheck(void);
/*******************************************************************************
* Variables
******************************************************************************/
uint8_t slaveRxData[TRANSFER_SIZE] = {0U};
uint8_t slaveTxData[TRANSFER_SIZE] = {0U};
dma_handle_t slaveTxHandle;
dma_handle_t slaveRxHandle;
spi_dma_handle_t slaveHandle;
volatile bool isTransferCompleted = false;
/*******************************************************************************
* Code
******************************************************************************/
static void SPI_SlaveUserCallback(SPI_Type *base, spi_dma_handle_t *handle, status_t status, void *userData)
{
if (status == kStatus_Success)
{
isTransferCompleted = true;
}
}
/*!
* @brief Main function
*/
int main(void)
{
/* Initialzie board setting. */
/* set BOD VBAT level to 1.65V */
POWER_SetBodVbatLevel(kPOWER_BodVbatLevel1650mv, kPOWER_BodHystLevel50mv, false);
/* attach 12 MHz clock to FLEXCOMM0 (debug console) */
CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);
BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitDebugConsole();
CLOCK_SetClkDiv(kCLOCK_DivPll0Clk, 0U, true);
CLOCK_SetClkDiv(kCLOCK_DivPll0Clk, 3U, false);
/* attach 50 MHz clock to HSLSPI */
CLOCK_AttachClk(kPLL0_DIV_to_HSLSPI);
/* reset FLEXCOMM for SPI */
RESET_PeripheralReset(kHSLSPI_RST_SHIFT_RSTn);
/* Print project information. */
PRINTF("This is SPI DMA transfer slave example.\r\n");
PRINTF("This example will communicate with another master SPI on the other board.\r\n");
PRINTF("Slave board is working...!\r\n");
/* Initialize the SPI slave instance. */
EXAMPLE_SlaveInit();
/* Configure DMA for slave SPI. */
EXAMPLE_SlaveDMASetup();
/* Start SPI DMA transfer. */
EXAMPLE_SlaveStartDMATransfer();
/* De-intialize the SPI instance. */
// SPI_Deinit(EXAMPLE_SPI_SLAVE);
while (1)
{
/* Waiting for transmission complete and check if all data matched. */
EXAMPLE_TransferDataCheck();
}
}
static void EXAMPLE_SlaveInit(void)
{
spi_slave_config_t slaveConfig;
/* Get default Slave configuration. */
SPI_SlaveGetDefaultConfig(&slaveConfig);
/* Initialize the SPI slave. */
slaveConfig.sselPol = (spi_spol_t)EXAMPLE_SLAVE_SPI_SPOL;
// slaveConfig.direction = kSPI_LsbFirst;
SPI_SlaveInit(EXAMPLE_SPI_SLAVE, &slaveConfig);
}
static void EXAMPLE_SlaveDMASetup(void)
{
/* DMA init */
DMA_Init(EXAMPLE_DMA);
/* configure channel/priority and create handle for TX and RX. */
DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_TX_CHANNEL);
DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_RX_CHANNEL);
DMA_SetChannelPriority(EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_TX_CHANNEL, kDMA_ChannelPriority0);
DMA_SetChannelPriority(EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_RX_CHANNEL, kDMA_ChannelPriority1);
DMA_CreateHandle(&slaveTxHandle, EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_TX_CHANNEL);
DMA_CreateHandle(&slaveRxHandle, EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_RX_CHANNEL);
}
static void EXAMPLE_SlaveStartDMATransfer(void)
{
uint32_t i = 0U;
/* Initialzie the transfer data */
for (i = 0U; i < TRANSFER_SIZE; i++)
{
slaveTxData[i] = 0U;
slaveRxData[i] = 0U;
}
/* Create handle for slave instance. */
SPI_SlaveTransferCreateHandleDMA(EXAMPLE_SPI_SLAVE, &slaveHandle, SPI_SlaveUserCallback, NULL, &slaveTxHandle,
&slaveRxHandle);
}
static void EXAMPLE_TransferDataCheck(void)
{
static status_t state = kStatus_Success;
uint32_t i = 0U, errorCount = 0U;
spi_transfer_t slaveXfer;
static bool aborted = false;
/* Initialzie the transfer data */
for (i = 0U; i < TRANSFER_SIZE; i++)
{
if(state != kStatus_Success)
{
slaveTxData[i] = 0x55;
}
else
{
slaveTxData[i] = 0x88/*slaveRxData[i]*/;
}
}
slaveXfer.txData = (uint8_t *)&slaveTxData;
slaveXfer.rxData = (uint8_t *)&slaveRxData;
slaveXfer.dataSize = 2 * TRANSFER_SIZE * sizeof(slaveTxData[0]);
slaveXfer.configFlags = kSPI_FrameAssert;
/* Start transfer, when transmission complete, the SPI_SlaveUserCallback will be called. */
state = SPI_SlaveTransferDMA(EXAMPLE_SPI_SLAVE, &slaveHandle, &slaveXfer);
isTransferCompleted = false;
if (kStatus_Success != state)
{
PRINTF("There is an error when start SPI_SlaveTransferDMA \r\n");
SPI_MasterTransferAbortDMA(EXAMPLE_SPI_SLAVE, &slaveHandle);
aborted = true;
}
else
{
aborted = false;
}
if(!aborted)
{
/* Wait until transfer completed */
while (!isTransferCompleted)
{
}
isTransferCompleted = false;
PRINTF("\r\nThe transmitted data are now:");
for (i = 0; i < TRANSFER_SIZE; i++)
{
if ((i & 0x0FU) == 0U)
{
PRINTF("\r\n ");
}
PRINTF(" 0x%02X", slaveTxData[i]);
}
PRINTF("\r\nThe received data are now:");
/*Check if the data is right*/
for (i = 0; i < TRANSFER_SIZE; i++)
{
/* Print 16 numbers in a line */
if ((i & 0x0FU) == 0U)
{
PRINTF("\r\n ");
}
PRINTF(" 0x%02X", slaveRxData[i]);
/* Check if data matched. */
if (slaveTxData[i] != slaveRxData[i])
{
errorCount++;
}
}
if (errorCount == 0)
{
PRINTF("\r\nSPI transfer all data matched! \r\n");
}
else
{
PRINTF("\r\nError occurred in SPI transfer ! \r\n");
}
}
}