LPC2XXX supported in MCUXpresso?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC2XXX supported in MCUXpresso?

402 Views
guillem_coromin
Contributor I

Hello, 

Let's see if somebody can clarify something for me:

I'd like to use MCUXpresso for a LPC2XXX. Family LPC2XXX is not among the supported devices.

In one of the bullet points in the overview states 'Built-in support for LPC Cortex-M MCUs, as per LPCXpresso IDE v8.22'

 

LPC2XXX family is among the supported devices for LPCXpresso...

Is LPC2XXX supported or not by MCUXpresso?

Thanks

Tags (1)
0 Kudos
1 Reply

341 Views
lpcxpresso_supp
NXP Employee
NXP Employee

LPC2xxx MCUs are based on older ARM cpus (typically ARM7TDMI), rather than on Cortex-M cpus. They are thus not supported in MCUXpresso IDE.

Regards,

MCUXpresso IDE Support

0 Kudos