It appears that the MCUXpresso Config tools for Peripherals does not support the MKE02Z16VLD4 Micro - What are the alternatives (different Micro is not an option)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

It appears that the MCUXpresso Config tools for Peripherals does not support the MKE02Z16VLD4 Micro - What are the alternatives (different Micro is not an option)

600 Views
billsousan
Contributor I

We are building a new design based on the MKE02Z16VLD4 processor.  NXP recommends using the MCUXpresso IDE for this chip (versus the old KDS). However, I saw where the Config tools for the MCUXpresso does not support the peripheral drivers.  So does this mean we have to write our own (is there example code since this is normally auto-generated)?  Are there other options? 

Thanks,

Bill

1 Reply

503 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bill,

That MCU is not supported yet.

MCU is not supported KE02.png

You can refer the driver_examples in SDK_2.3.0_MKE02Z16xxx4. The MCUXpresso SDK API Reference Manual_MKE02Z4 is in docs folder(C:\SDK_2.3.0_MKE02Z16xxx4\docs).

SDK_2.3.0_MKE02Z16xxx4 driver_examples.PNG

MCUXpresso SDK API Reference Manual_MKE02Z4.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos