Installing MCUXpresso on non-internet connected computer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing MCUXpresso on non-internet connected computer

1,252件の閲覧回数
joseph_lindula
Contributor IV

Hello, I need some help installing MCUXpresso on a computer that is not connected to the internet. I was able to download the installation file from my internet computer and install it on my non-internet computer. When I try to create a project I don't see any available devices. 

Are there any packages that I need to download and install?

 

Thank you

Joe

0 件の賞賛
返信
3 返答(返信)

1,173件の閲覧回数
joseph_lindula
Contributor IV

Hello, I'm looking at using this device: LPC1112FDH28/102:5. 

0 件の賞賛
返信

1,153件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @joseph_lindula 

Please import lpcopen demo refer to the video in my attachment. 

If there is no LPCopen under MCUXpresso IDE installation directory. Please download from:

https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true 

Then copy it to your PC. Refer to the video in attachment to import demo and create new project.

If still have any issue, please contact me.

 

BR

Alice

0 件の賞賛
返信

1,226件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @joseph_lindula 

Which chip you use? 

There are two main categories of MCUs supported by MCUXpresso IDE. Preinstalled and via SDKs. Detail please refer to MCUXpresso IDE User Guide -> 4 Part support overview (preinstalled and via SDKs). 

 

BR

Alice

0 件の賞賛
返信