Hi ,
Am using IMXRT 1050 KVKB
Application : emWIN
Compiler : MCUxpresso
I generated (.sb) file using MCUXpresso file size is 2 MB
using MFG Tool if i flash our IMXRT EVKB it is not flashing and showing errror in MFG_LOG file
" "description" : "10203 (0x27DB) kStatusMemoryCumulativeWrite",
"ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)"
Currently am flashing in Hyper flash size of hyper flash in board is 32MB.
i have attached MFG Error picture and log file
Thanks in advance for your reply.
Regards,
Rizwan M
Hello Rizwan M,
What about your version of SDK and DAP-LINK ? You can refer to the below thread to check:
Programming i.MXRT with MCUXpresso IDE and BOOT
And then use the latest SDK and DAP-link try again. Using steps the DOC list:
3. Using MFGTool program with Boot .
From the SDK2.3.1, projects and its generated *.bin file include XIP files that add this information to the project,
so we can use MFG directly flash it to external flash .
Hope it helps,
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------