I2C : NO clock signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C : NO clock signal

1,707 Views
sendhilkumar_ha
Contributor I

Hi,

Iam working on I2c communication with LP5024 LED.

K22 will be the master and need to communicate with LP5024 slave.

 I2C SDK driver : downloaded from https://mcuxpresso.nxp.com/en/builder#

Iam able to Initialize I2C via I2C_MasterInit API and   I2C_MasterStart, I2C_MasterTransferBlocking calls were successful

Issue is that iam not seeing clock signal in oscilloscope. Am i missing anything? Below is the code i used for I2C master. Kindly go through and advise me how to proceed with this issue.

 

 Please suggest.

                status_t result = kStatus_Success;
                I2C_MemMapPtr base = I2C0_BASE_PTR;
                i2c_master_config_t masterConfig = {0};
                I2C_MasterGetDefaultConfig(&masterConfig);
                uint8 status;

                I2C_MasterInit(base, &masterConfig, 100000U);

                /* Clear all status before transfer. */
                I2C_MasterClearStatusFlags(base, (uint32_t)(kClearFlags));
                /* Clear pending flag. */
                base->S = (uint8_t)kI2C_IntPendingFlag;


                result = I2C_MasterStart(base, 0x00, kI2C_Write);

                if (0 != result)
                {
                                result = kStatus_Fail;
                }

                /* Wait address sent out. */
                if(!((status = I2C_MasterGetStatusFlags(base)) & kI2C_IntPendingFlag))
                {
                }

                if(status & kI2C_ReceiveNakFlag)
                {                
                }

                /* Enable module interrupt. */
                I2C_EnableInterrupts(base, kI2C_GlobalInterruptEnable);


                result = kStatus_Success;
                result = I2C_MasterWriteBlocking(base, txBuff, BUFFER_SIZE, kI2C_TransferNoStopFlag);
                if (result)
                {
                                I2C_MasterStop(base);
                }

Regards,

SK

Tags (1)
0 Kudos
Reply
4 Replies

1,546 Views
sendhilkumar_ha
Contributor I

Thanks Alexis. 

Issue resolved.

Regards,

Sendhil

0 Kudos
Reply

1,546 Views
sendhilkumar_ha
Contributor I

Thanks Alexis.

Yes, i updated the Board_InitPins as below: 

With some added code, iam able to see the SDA pin going low when START signal is sent from I2C_MasterStart

void BOARD_InitPins(void)
{
           /* Port E Clock Gate Control: Clock enabled */ 
          CLOCK_EnableClock(kCLOCK_PortE);
         /* PORTE24 (pin 31) is configured as I2C0_SCL */
          PORT_SetPinMux(PORTE_BASE_PTR, 24U, kPORT_MuxAlt5);
 
         PORTE_BASE_PTR->PCR[24] = ((PORTE_BASE_PTR->PCR[24] &       
                    (~(PORT_PCR_PS_MASK | PORT_PCR_PE_MASK | PORT_PCR_ODE_MASK | PORT_PCR_ISF_MASK)))
                    | (uint32_t)(kPORT_PullUp)
                    | PORT_PCR_ODE(kPORT_OpenDrainDisable));
 
        /* PORTE25 (pin 32) is configured as I2C0_SDA */
         PORT_SetPinMux(PORTE_BASE_PTR, 25U, kPORT_MuxAlt5);
 
         PORTE_BASE_PTR->PCR[25] = ((PORTE_BASE_PTR->PCR[25] &
                  (~(PORT_PCR_PS_MASK | PORT_PCR_PE_MASK | PORT_PCR_ISF_MASK)))
                 | (uint32_t)(kPORT_PullUp));
 
 
        const port_pin_config_t porte24_pin31_config = {
                  kPORT_PullUp, /* Internal pull-up resistor is enabled */ 
                  kPORT_FastSlewRate, /* Fast slew rate is configured */ 
                  kPORT_PassiveFilterDisable, /* Passive filter is disabled */ 
                  kPORT_OpenDrainEnable, /* Open drain is enabled */ 
                  kPORT_LowDriveStrength, /* Low drive strength is configured */ 
                  kPORT_MuxAlt5, /* Pin is configured as I2C0_SCL */ 
                  kPORT_UnlockRegister /* Pin Control Register fields [15:0] are not locked */
          };
 
          /* PORTE24 (pin 31) is configured as I2C0_SCL */
          PORT_SetPinConfig(PORTE_BASE_PTR, 24U, &porte24_pin31_config);

        const port_pin_config_t porte25_pin32_config = {
                  kPORT_PullUp, /* Internal pull-up resistor is enabled */ 
                  kPORT_FastSlewRate, /* Fast slew rate is configured */ 
                  kPORT_PassiveFilterDisable, /* Passive filter is disabled */ 
                  kPORT_OpenDrainEnable, /* Open drain is enabled */ 
                   kPORT_LowDriveStrength, /* Low drive strength is configured */ 
                   kPORT_MuxAlt5, /* Pin is configured as I2C0_SDA */ 
                   kPORT_UnlockRegister}; /* Pin Control Register fields [15:0] are not locked */
         /* PORTE253 (pin 32) is configured as I2C0_SDA */
          PORT_SetPinConfig(PORTE_BASE_PTR, 25U, &porte25_pin32_config);
}

It is waiting in while loop on I2C_MasterTransferBlocking 

             #if I2C_WAIT_TIMEOUT
                  ...
             #else
                    /* Wait until data transfer complete. */
                   while (0U == (base->S & (uint8_t)kI2C_IntPendingFlag))
                  {
                  }
             #endif

this is my main code: Kindly advise if iam missing anything

void i2c_init()
{
  uint8 status;
  status_t result = kStatus_Success;
  I2C_MemMapPtr *i2cch = I2C0_BASE_PTR;
  i2c_master_config_t masterConfig = {0};
  masterConfig.baudRate_Bps = I2C_BAUDRATE;
  i2c_master_transfer_t masterXfer;

  BOARD_InitPins();

  I2C_MasterGetDefaultConfig(&masterConfig);


  I2C_MasterInit(i2cch, &masterConfig, 36864000);

  I2C_Enable(i2cch, false);
  I2C_Enable(i2cch, true);

  /* Clear pending flag. */
  i2cch->S = (uint8_t)kI2C_IntPendingFlag;

  result = I2C_MasterStart(i2cch, 0x28U, kI2C_Write);

if (0 != result)
{
result = kStatus_Fail;
}

/* Wait address sent out. */
if(!((status = I2C_MasterGetStatusFlags(i2cch)) & kI2C_IntPendingFlag))
{
}

 if(status & kI2C_ReceiveNakFlag)
 {
 }

  /* Enable module interrupt.*/
  I2C_EnableInterrupts(i2cch, kI2C_GlobalInterruptEnable);


  result = kStatus_Success;

  uint8_t g_master_txBuff[I2C_DATA_LENGTH];
  memset(&g_m_handle, 0, sizeof(g_m_handle));

  /* subAddress = 0x01, data = g_master_txBuff - write to slave.
  start + slaveaddress(w) + subAddress + length of data buffer + data buffer + stop*/
  uint8_t deviceAddress = 0x28U;
  masterXfer.slaveAddress = I2C_MASTER_SLAVE_ADDR_7BIT;
  masterXfer.direction = kI2C_Write;
  masterXfer.subaddress = (uint32_t)deviceAddress;
  masterXfer.subaddressSize = 1;
  masterXfer.data = g_master_txBuff;
   masterXfer.dataSize = I2C_DATA_LENGTH;  
  masterXfer.flags = kI2C_TransferDefaultFlag;
  result = I2C_MasterTransferBlocking(i2cch, &masterXfer);
  if (result)
 {
    I2C_MasterStop(i2cch);
 }
}

0 Kudos
Reply

1,546 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Sendilkumar,

The pin initialization looks good but after checking your code I saw that this sentences are repeated:

  /* Clear pending flag. */
  i2cch->S = (uint8_t)kI2C_IntPendingFlag;

  result = I2C_MasterStart(i2cch, 0x28U, kI2C_Write);

if (0 != result)
{
result = kStatus_Fail;
}

/* Wait address sent out. */
if(!((status = I2C_MasterGetStatusFlags(i2cch)) & kI2C_IntPendingFlag))
{
}

 if(status & kI2C_ReceiveNakFlag)
 {
 }

  /* Enable module interrupt.*/
  I2C_EnableInterrupts(i2cch, kI2C_GlobalInterruptEnable);


  result = kStatus_Success;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

This process is already done in the I2C_MasterTransferBlocking so you wouldn't need it for it.

If you want to enable the interruption I will suuggest to check the example frdmk22f_i2c_interrupt_b2b_transfer_master. 

Best Regards,

Alexis Andalon

1,546 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Sendhilkumar,

Did you have in count the initialization of the pin? For example, in the SDK example, in the BOARD_InitPins API the I2C are initialized so I will suggest to check this function.

Also, I saw that you're using a simplified version of the I2C_MasterWriteBlocking/I2C_MasterWriteNonBlocking but you're omitting some flags that could be need it for the proper functionality of the module so I will suggest to use this two functions instead.

Let me know if this helps you.

Best Regards,
Alexis Andalon

0 Kudos
Reply