How to download axf file to LPC1769 based PCB board by using LPC Link 2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to download axf file to LPC1769 based PCB board by using LPC Link 2?

ソリューションへジャンプ
1,858件の閲覧回数
changwenxie
Contributor I

I am using LPCXpresso to develop and debug the application program running at LPC1769.

I can download the code to LPC1769 based PCB by using LPC - Link 2 and a customer inter-connection board and debug the code from the development environment (LPCXpresso).

Now, I need to know which software (not the development environment tool LPCXpresso) will be used to download the pre-build axf file into the product hardware (LPC1769 based PCB) by using LPC - Link 2 in the production line?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,795件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Changwen Xie ,

Sorry as far as I know, there isn't a tool to download with LPC-link2 except IDE.

While there is a "GUI Flash Tool" inside LPCXpresso IDE, it can directly download file:

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,796件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Changwen Xie ,

Sorry as far as I know, there isn't a tool to download with LPC-link2 except IDE.

While there is a "GUI Flash Tool" inside LPCXpresso IDE, it can directly download file:

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,795件の閲覧回数
changwenxie
Contributor I

Thank you very much.

Do you know is there any plan in future to split the programming the flash tool as a tool?

Kind regards

Changwen Xie

0 件の賞賛
返信