How to download axf file to LPC1769 based PCB board by using LPC Link 2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to download axf file to LPC1769 based PCB board by using LPC Link 2?

跳至解决方案
1,951 次查看
changwenxie
Contributor I

I am using LPCXpresso to develop and debug the application program running at LPC1769.

I can download the code to LPC1769 based PCB by using LPC - Link 2 and a customer inter-connection board and debug the code from the development environment (LPCXpresso).

Now, I need to know which software (not the development environment tool LPCXpresso) will be used to download the pre-build axf file into the product hardware (LPC1769 based PCB) by using LPC - Link 2 in the production line?

Thanks

标签 (1)
0 项奖励
回复
1 解答
1,888 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Changwen Xie ,

Sorry as far as I know, there isn't a tool to download with LPC-link2 except IDE.

While there is a "GUI Flash Tool" inside LPCXpresso IDE, it can directly download file:

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,889 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Changwen Xie ,

Sorry as far as I know, there isn't a tool to download with LPC-link2 except IDE.

While there is a "GUI Flash Tool" inside LPCXpresso IDE, it can directly download file:

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,888 次查看
changwenxie
Contributor I

Thank you very much.

Do you know is there any plan in future to split the programming the flash tool as a tool?

Kind regards

Changwen Xie

0 项奖励
回复