How to debug bootloader and application codes together in MCUXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to debug bootloader and application codes together in MCUXpresso

跳至解决方案
5,641 次查看
MAPC
Senior Contributor I

Hello,

Some time ago, it was posted a tutorial about how to debug bootloader and application code together in KDS.Debugging Bootloader and Application using Kinetis Design Studio.  I have tried to follow the its steps, using .axf file, instead of .elf file, but it didn't work.

Could anybody tell me how to do it in MCUXpresso?

Thanks and best regards,

Marco Coelho

DFAE - Siletec Eletronica

1 解答
4,251 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Marco,

Which debug connection are you using? I have done a quick test using the Jlink connection and I'm able to debug both  projects by adding this command to the debug Run Commands:

add-symbol-file C:\\Users\\b38285\\Documents\\MCUXpressoIDE_10.0.0_344\\workspace\\MK64FN1M0xxx12_Project_2\\Debug\\MK64FN1M0xxx12_Project_2.axf 0x80000

pastedImage_1.png

The address 0x80000 corresponds to the first flash section of the second project which was previously flashed to the MCU:

pastedImage_3.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

在原帖中查看解决方案

3 回复数
4,252 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Marco,

Which debug connection are you using? I have done a quick test using the Jlink connection and I'm able to debug both  projects by adding this command to the debug Run Commands:

add-symbol-file C:\\Users\\b38285\\Documents\\MCUXpressoIDE_10.0.0_344\\workspace\\MK64FN1M0xxx12_Project_2\\Debug\\MK64FN1M0xxx12_Project_2.axf 0x80000

pastedImage_1.png

The address 0x80000 corresponds to the first flash section of the second project which was previously flashed to the MCU:

pastedImage_3.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

4,251 次查看
MAPC
Senior Contributor I

Well, that's embarrassing, Carlos!

I simply inserted the wrong application's path in Debug Configurations! I can't believe I committed such a mistake.

Sorry for bothering you with that.

Regards,

Marco Coelho

DFAE - Siletec Eletronica

0 项奖励
回复
4,251 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Marco,

 

No problem, it is good to hear that it is now working correctly.

 

Best Regards!
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复