Hello,
I want to get analog sensor values using NXP board "TWR-KE18F".
However, it is not done for the following reasons.
- I don't know much about the hardware, so I don't know how to connect the board and sensor.
How can I connect the board and sensor?
- I don't know the code to use the external analog sensor.
Please tell me the sample code to get the value of external analog sensor.
I understand how to get the value of the potentiometer attached to the board in the SDK sample project “adc12_polling”.
However, the code that uses an external analog sensor is not known.
Notes:
I have the "TWR-ELEV" and "TWR-PROTO" necessary to configure the tower module.
I have external sensors such as light sensors and temperature sensors.
Best regards.