GDB PEMicro interface debugging not showing up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GDB PEMicro interface debugging not showing up

820 Views
catalin_iordach
Contributor I

Hi,

I recently installed Kinetis Deign Studio 3.2.0 on Mac OSX High Sierra and am I trying to flash a FRDM-KL26Z (am studying this at the University and everybody use Windows, unfortunatly).

I installed the GDB PEMicro packs, but the problem is that the only configuration that shows up into the Flash Configurations is GDB Segger J-Link Debugging. 

I've tried to select and deselect several options from Launch Configurations, without succes; the only thing that changes is J-Link dissapearing from Flash Configurations.

Any help, or suggestions?

gdb.png

Labels (1)
0 Kudos
Reply
1 Reply

671 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Catalin

In the Release notes of the KDS 3.2 there is a note that mentioned:

pastedImage_1.png

So, for MAC, you only have support for Segger interface. I would like to recommend you MCUXpresso IDE which has full support for LinkServer, P&E or SEGGER.

Best regards

Jorge Alcala

0 Kudos
Reply