Fail to install OpenSDA probe firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fail to install OpenSDA probe firmware

1,823 次查看
qian990612
Contributor I

I have been having trouble running example programs on my IMXRT1050-EVKB. I kept getting error

Unable to connect wire for probe index 1

Error: Wire Ack Fault - target connected?

So I tried to download OpenSDA probe firmware according to this post but after I dropped the firmware to the board, I got a FAIL.txt containing the following message:

The application file format is unknown and cannot be parsed and/or processed.

I am wondering what I should do to fix this problem

Board: IMXRT1050-EVKB

IDE: MCUXpresso IDE v11.2.0_4120

SDK: SDK 2.8.0 for EVKB-IMXRT1050

OS: Windows 10

0 项奖励
回复
2 回复数

1,767 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

Could you please confirm if you are following same steps described in chapter 5 of the community document below?

 

https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2017/12/07/overview-of-using-the-... 

 

Regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 项奖励
回复

1,758 次查看
qian990612
Contributor I

I followed the instruction to download the firmware. Now I am not getting FAIL.txt, but I am still getting the same error when trying to connect to the board.

0 项奖励
回复