I know this is a very old topic. I found a lot of "answers" in the nxp or eclipse forum. unfornately none of them can help me out of the issue
My IDE: MCUXpressor
All the setup are default from origin
SDK:
Issue: I am trying to tracking the "TaskFunction", but it stucks.
I follow some "old advise" from this forum to change the indexer setup:
Unfortunately, this move doesn't help me at all.
Everytime I met this situation, I have to use the "search text" function to find the element violently. It works, but very inefficient
Can anyone here help?
Did you already follow the steps in https://mcuoneclipse.com/2012/03/20/fixing-the-eclipse-index/ ?
The other hint is that it might be related to the line count of your source files: see https://mcuoneclipse.com/2012/08/07/eclipse-editor-scalability/ , so you might increase that 5'000 to something like 10'000, because at least one FreeRTOS file is larger than 5k lines.
I hope this helps,
Erich
Both articles unfortunately still apply to the latest Eclipse version.
What I can tell from my side that disable heuristics and increasing the scalability value is solving that exact problem on my side. I just have verified it with the MCUXpresso IDE 11.6.1, and with that settings it is able to locate TaskFunction_t.
As this seems not to work on your end, you could check the indexer debug option: https://mcuoneclipse.com/2021/01/10/eclipse-indexer-debug-tips/
Maybe this gives a hint to you what is going wrong?
I hope this helps,
Erich