Error reported by target when MCU is in low power mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error reported by target when MCU is in low power mode

308 Views
BLEDev
Contributor II

Hello NXP,

 

BLEDev_1-1729594019316.png

When I start debugging mode then hit "resume" BLEDev_2-1729594677864.png and wait SW enters deep sleep mode (KW45 MCU) immediately above error dialog appears. After a wakeup source triggered, I have to click "OK" to close the dialog windows then I can continue debug SW, which is inconvenient. I want to continue debugging in deep sleep mode without this interruption (I want to trigger wakeup sources to see software behavior swhen entering/exiting deep sleep mode).  In IAR, a similar dialog only appears if the software is already in deep sleep mode, and I hit "Break" as below

BLEDev_3-1729595206662.png

BLEDev_4-1729595245178.png

 

How can I achieve the similar behavior as in IAR?

 

Thanks!

0 Kudos
Reply
1 Reply

263 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. As working with low power mode, it would depend on the specific power mode if the SWD is disabled or not, and it is as expected behavior on the IDE when loosing SWD communication.

 

Regards,

Ricardo

0 Kudos
Reply