Did any one success run FlexCan Interrupt demo in SDK2.0 for MK22F120?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Did any one success run FlexCan Interrupt demo in SDK2.0 for MK22F120?

1,015 次查看
changfuzhao
Contributor III

I am try to running flexcan interrupt (two board) demo in sdk2.0 for MK22FN120, but I never got success, 

and more please let me know what is difference between MK22FN1M0Axxx12 and MK22FN1M0xxx12?

0 项奖励
2 回复数

756 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Changfu Zhao

We recommend to use the latest SDK drivers in order to avoid any possible bug on older versions. I could run the flexcan_interrupt driver example code for twrk21f120m following the readme file.

About your other question, please check the following link:

https://community.nxp.com/docs/DOC-102548 

Hope this could help you.

Best Regards

Jorge Alcala

0 项奖励

756 次查看
changfuzhao
Contributor III

thanks for your reply,

I used SDK2.2 now, and my MCU is MK22FN1M0VLH12,

I port the demo from twrk21f120m to my board, and run it talk to my CAN bus device by 250k, but, I didn't  success by many times. but I can use Process Expert generate code and success communication to my device.

I just think may be the bit rate calculation in SDK has some thing wrong.

0 项奖励