I'm debugging an application running on the M7 core of the IMXRT1176 MCU. I'm trying to view the DMA0 and DMAMUX0 peripheral registers but noticed they are not visible in the peripherals viewer. DMA1 and DMAMUX1 are, however, I think these are only available on the M4 core. Can someone tell me how to view the peripherals I want.
Thank you for the reply. The examples show the correct peripherals for me. It's just our project that has the issue and I can't find the difference in the project configuration that would cause this.
If you can see the peripherals/registers without problem running the SDK examples, please verify that your application is actually running in the M7 core.
DMA0 and DMAMUX0 are available in Cortex-M7. DMA1 and DMAMUX1 are available in Cortex-M4.