Compiler error "No such file or directory"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Compiler error "No such file or directory"

跳至解决方案
2,330 次查看
Thomas_Kroll
Contributor I

Hello community,

I have get a non telling compiler error message and could not find the reason for it.
I'm using MCUXpresso IDE v11.7.0 [Build 9198] [2023-01-17]

Content of the build logging file:

11:00:38 **** Incremental Build of configuration Debug for project MoReTi_V1_00 ****
make -r all
Building file: ../utilities/fsl_assert.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -std=gnu99 -D__REDLIB__ -DSD_ENABLED -DFSL_RTOS_FREE_RTOS -DCPU_MIMXRT1176CVM8A -DCPU_MIMXRT1176CVM8A_cm7 -DXIP_BOOT_HEADER_DCD_ENABLE=0 -DUSE_SDRAM -DDATA_SECTION_IS_CACHEABLE=1 -DSDK_DEBUGCONSOLE=1 -DXIP_EXTERNAL_FLASH=0 -DXIP_BOOT_HEADER_ENABLE=0 -DPRINTF_FLOAT_ENABLE=1 -DSCANF_FLOAT_ENABLE=0 -DPRINTF_ADVANCED_ENABLE=0 -DSCANF_ADVANCED_ENABLE=0 -DFSL_SDK_DRIVER_QUICK_ACCESS_ENABLE=1 -DMCUXPRESSO_SDK -DCR_INTEGER_PRINTF -D__MCUXPRESSO -D__USE_CMSIS -DDEBUG -DSDK_OS_FREE_RTOS -DSERIAL_PORT_TYPE_UART=1 -DSKIP_DCDC_ADJUSTMENT = 1 -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\board" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\CMSIS" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\component\crc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\component\lists" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\component\osa" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\component\serial_manager" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\component\uart" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\device" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\drivers" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\drivers\freertos" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\AFE 13388\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\AFE 13388\SPI\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\CAN\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\Digital_IO\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\EEPROM\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\FLEXSPI_Flash\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\Hello_World\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\I2C\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\IOT\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\LCD_Display_RK055x\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\LED Blinky\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\PMIC\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\PortExpander\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\RS485\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\SEMC\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\Example\UART\Inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\freertos\RTOS_Config" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\freertos\TASK_Manage" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\lwip\contrib\apps\ping" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\lwip\port" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\lwip\src" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\lwip\src\include" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\sdmmc\host" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\sdmmc\inc" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\sdmmc\osa" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\source" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\startup" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\trustzone" -I"H:\Cortex\MoReTi\WSP1\MoReTi_V1_00\utilities" -Og -fno-common -g3 -c -ffunction-sections -fdata-sections -ffreestanding -fno-builtin -fmacro-prefix-map="../utilities/"= -mcpu=cortex-m7 -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -D__REDLIB__ -fstack-usage -specs=redlib.specs -MMD -MP -MF"utilities/fsl_assert.d" -MT"utilities/fsl_assert.o" -MT"utilities/fsl_assert.d" -o "utilities/fsl_assert.o" "../utilities/fsl_assert.c"
arm-none-eabi-gcc: error: =: No such file or directory
arm-none-eabi-gcc: error: 1: No such file or directory
make[1]: *** [utilities/subdir.mk:26: utilities/fsl_assert.o] Error 1
make: *** [makefile:79: all] Error 2
"make -r all" terminated with exit code 2. Build might be incomplete.

11:00:40 Build Failed. 2 errors, 0 warnings. (took 2s.129ms)

 

Thanks, for your help!

0 项奖励
回复
1 解答
2,323 次查看
ErichStyger
Specialist I

Remove the two spaces in your command line here:

ErichStyger_0-1680091496571.png

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,324 次查看
ErichStyger
Specialist I

Remove the two spaces in your command line here:

ErichStyger_0-1680091496571.png

 

0 项奖励
回复
2,313 次查看
Thomas_Kroll
Contributor I
This was exactly the solution. Many thank for your help.
0 项奖励
回复