Cannot update MCULink firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot update MCULink firmware

ソリューションへジャンプ
3,221件の閲覧回数
leannee
Contributor II

Hello.

I have a strange problem with MCULink on LPCXpresso55s36 board. OS is Windows 10.

I should highlight that I have successfully programmed it under Ubuntu.

I simply cannot update MCULink firmware under Windows. The board is in ISP mode. The board is detected and enumerated as HID-compliant vendor-define device.

When running program_CMSIS.cmd (or JLINK, no difference), the script is stuck when I press "any key" (so the script doesn't even complain it cannot find the probe/the probe is not in ISP mode etc.).

Trying to debug the problem, I went to blhost (with admin rights) and ran a line from *.cmd script: 

blhost.png

That's it, nothing happens after that. Moreover, I cannot close the powershell, and blhost.exe process is absolutely unkillable.

What I can guess, the problem is related to permissions, access rights etc. But no response from blhost makes it super hard to track. Also I am not sure where to even look for permissions for USB...

Summary:

blhost doesn't get reply from MCULink AND hangs forever without any response, the process is unkillable. Ctrl+C doesn't help too.

I could not find any posts even remotely like that, so I am very curious about the reason for such behavior.

EDIT: By the way, after updating MCULink (CMSIS) from Ubuntu, I can program MCU just fine from Windows + MCUXpresso IDE.

0 件の賞賛
返信
1 解決策
3,036件の閲覧回数
leannee
Contributor II

First of all, firewall has nothing to do with it. That's not how blhost works.

I disabled it anyway. No luck. Reinstalling? Tried several times with several versions.

Okay, I've opened the source code of blhost, and then of libusbsio. Figured out the exact line where the process hangs (inside hid_write_timeout function for anyone wondering).

Thanks to Visual Studio Debugger, I have identified what process/program interferes with blhost in such a weird way. Not going to name it, but it is indeed (partially) security-related. It was not obvious, though! Uninstalled (though I think simply killing the related process before running blhost would be enough) and blhost FINALLY works.

This was too specific, and would hardly happen again to anyone. Otherwise - go and debug the code yourself, it is the only way.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,151件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @leannee 

Do you refer to the steps below?

Alice_Yang_0-1697447854367.png

 

What about the version of your board? The version of MCU-link installer? Please take a video about the steps on your side.

 

BR

Alice

 

 

0 件の賞賛
返信
3,142件の閲覧回数
leannee
Contributor II

Yes, I refer to these steps. Which I follow to the dot. The board is in ISP mode: D16 is on, the board is enumerated as HID device (VID 0x1FC9, PID 0x0021).

I have no idea about the version of the board. Although the marking says WO-**-2308, which I guess yyww?So it should be fresh. Both MCUs are from last year, based on markings.

I have tried version 3.108 of MCULink installer.

I repeat, I have successfully updated the MCULink firmware to version 3.108 using Ubuntu.

 

0 件の賞賛
返信
3,132件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @leannee 

I tested on my side, win10, MCULink firmware to version 3.108 /3.122, there is no problem:

Alice_Yang_0-1697510343743.png

 

Do you have other win10 PC, you can test with another PC.

 

BR

Alice

 

 

0 件の賞賛
返信
3,127件の閲覧回数
leannee
Contributor II

Hello, @Alice_Yang .

Thank you. Of course it is working fine. It is not supposed to happen, otherwise it would have been mentioned already by other users.

That was not my question anyway.

I have even tested it on another PC in my company, guessing it might be security software interfering, but it worked (updating MCULink firmware with program_CMSIS.cmd via blhost).

USB ports and cables on my PC are also okay: I can (now) flash and debug the target MCU in MCUXpresso IDE. However, the said MCULink firmware update tool is still not working on my PC.

So, again: I am not talking about bugs in software. My question is, let me clarify:

What might be the reason for blhost hanging with no response when get-property/set-property command is executed on Windows 10?

Simply curious.

0 件の賞賛
返信
3,095件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @leannee 

How about disable firewall ?

Or reinstall  MCU-link installer ?

 

BR

Alice

0 件の賞賛
返信
3,037件の閲覧回数
leannee
Contributor II

First of all, firewall has nothing to do with it. That's not how blhost works.

I disabled it anyway. No luck. Reinstalling? Tried several times with several versions.

Okay, I've opened the source code of blhost, and then of libusbsio. Figured out the exact line where the process hangs (inside hid_write_timeout function for anyone wondering).

Thanks to Visual Studio Debugger, I have identified what process/program interferes with blhost in such a weird way. Not going to name it, but it is indeed (partially) security-related. It was not obvious, though! Uninstalled (though I think simply killing the related process before running blhost would be enough) and blhost FINALLY works.

This was too specific, and would hardly happen again to anyone. Otherwise - go and debug the code yourself, it is the only way.

0 件の賞賛
返信