Hi,
Chip: MKE15Z256VLL7
MCUXpresso Version: 10.3.1
Debug Prober: SEGGER. SWD mode
If I run the program without suspended or breakpoint, it runs no problem. But if I suspend it manually or by setting a breakpoint, the program can not resume. It shows "Error: Command aborted." in debugger window. In Diassembly window shows "000018fc: Failed to execute MI command:
-data-disassemble -s 6396 -e 6428 -- 2
Error message from debugger back end:
Cannot access memory at address 0x18fc"
The code is running without FreeRTOS.
Thanks.
Hello Ran Tao,
How about a simple project , for example "hello world" ?
And please step by step to check which code make it crash.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------