Can not stop debug and dowload software with evkmimxrt1064_freertos_tickless

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not stop debug and dowload software with evkmimxrt1064_freertos_tickless

ソリューションへジャンプ
1,167件の閲覧回数
rickyrocky
Contributor I

Hi all,

I am using [evkmimxrt1064_freertos_tickless] sample of MCUXPresso IDE to test sleep mode.

After __WFI() has called in vPortSuppressTicksAndSleep()

I press [terminate] the debug, but can not stop it. And it is OK with [Terminate All Debug session].
Then I run debug again, but can't connect to the device.
 
Does debug work after __WFI()?, or do I need to configure anything related to it? 
 
[My environment]
Board i.MXRT1064
Using J-Link for downloading and debug
DCC 5v for suppling power
 
[Recovery method]
Change to Serial Download (SW7 0.0.0.1), then Erase All Chip by using J-Flash.
0 件の賞賛
返信
1 解決策
1,133件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @rickyrocky ,

  If you find the board can't connect the debugger, you can refer to this post to recover it:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta...

 About the low power code, I suggest you use this code in the SDK:

  \SDK_2_13_0_EVK-MIMXRT1064\boards\evkmimxrt1064\demo_apps\power_mode_switch\rtos

 

 If you still have questions about it, please use the company email to create the new question post, it will have higher priority than the 3rd part email.

Best Regards,

kerry

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,134件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @rickyrocky ,

  If you find the board can't connect the debugger, you can refer to this post to recover it:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta...

 About the low power code, I suggest you use this code in the SDK:

  \SDK_2_13_0_EVK-MIMXRT1064\boards\evkmimxrt1064\demo_apps\power_mode_switch\rtos

 

 If you still have questions about it, please use the company email to create the new question post, it will have higher priority than the 3rd part email.

Best Regards,

kerry

0 件の賞賛
返信